AXIS#.MT.TNEXT

Description

AXIS#.MT.TNEXTspecifies the time that must elapse before starting a following motion task.

Once a delay value has been entered, the transition type (AXIS#.MT.TRANSITION) must be set to 1. All other transitions types will not use the delay.

The motion task control word can be selected so that a following motion task is executed after a first motion task and this additional delay time.

Examples

Code

Sets the delay of motion task 0 to 10ms. The first parameter is the motion task number and the second is the delay in milliseconds

-->AXIS1.MT.TNEXT 0 10

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only Array

Units

ms

Range

0 to 65,535 ms

Default Value

0 ms

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.TNEXT 0

50d9h

01h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 1

50d9h

02h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 2

50d9h

03h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 3

50d9h

04h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 4

50d9h

05h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 5

50d9h

06h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 6

50d9h

07h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 7

50d9h

08h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 8

50d9h

09h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 9

50d9h

0ah

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 10

50d9h

0bh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 11

50d9h

0ch

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 12

50d9h

0dh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 13

50d9h

0eh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 14

50d9h

0fh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 15

50d9h

10h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 16

50d9h

11h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 17

50d9h

12h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 18

50d9h

13h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 19

50d9h

14h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 20

50d9h

15h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 21

50d9h

16h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 22

50d9h

17h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 23

50d9h

18h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 24

50d9h

19h

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 25

50d9h

1ah

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 26

50d9h

1bh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 27

50d9h

1ch

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 28

50d9h

1dh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 29

50d9h

1eh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 30

50d9h

1fh

Unsigned16

-

-

Read/Write

No

AXIS1.MT.TNEXT 31

50d9h

20h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6308

1

6308 (0x18a4)

AXIS1.MT.TNEXT

Unsigned16[32]

Read/Write

Yes

71844

2

6308 (0x18a4)

AXIS2.MT.TNEXT

Unsigned16[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.TNEXT

6308

Unsigned16[32]

Read/Write

-

Related Topics

Motion Tasks